When creating products in hazardous locations, there are various regulatory bodies to keep in mind. There are standards driven organizations that outline the parameters for devices in hazardous locations. For example, this would be IEC 60079. In addition to or as an alternative, regional based standards are also at play. For example, in the US, NEC and UL drive the Class 1 Divison 2 standard which is a common benchmark for equiptment in hazardous locations. In general, there are many synergies across all these standards.