Maker.io main logo

AI-Powered Waste Segregation with Arduino UNO Q

2026-06-12 | By Rinme Tom

License: GNU Lesser General Public License Arduino

Build a Computer Vision System That Automatically Sorts Waste

Waste segregation is one of the simplest ways to improve recycling efficiency, yet it is often overlooked in everyday life. Mixing paper, plastic, cardboard, and batteries in the same container makes recycling more difficult and can lead to environmental contamination. In this project, we build an AI-powered waste segregation system that automatically identifies common waste materials and directs them to the appropriate collection area.

Using an Arduino UNO Q, a USB camera, and an object detection model trained with Edge Impulse, the system recognizes different waste categories in real time. Once an item is identified, a servo motor directs it to the correct bin, while hazardous items such as batteries trigger an audible warning.

Automatic Waste Segregation System

How the System Works

The Automatic Waste Segregation System project combines embedded hardware with computer vision to create a compact automated sorting system.

A USB camera continuously captures images of incoming waste items. These images are processed using an object detection model trained to recognize four categories:

  • Paper

  • Cardboard

  • Plastic

  • Battery

The trained model runs through the Arduino App Lab environment and analyzes each video frame. To improve reliability, detections must appear consistently across multiple frames before the system takes action. This reduces false triggers caused by lighting variations, object movement, or temporary misclassifications.

Once a valid detection is confirmed, commands are sent to the Arduino UNO Q through RouterBridge. The microcontroller then controls a servo motor or buzzer based on the detected waste type.

Hardware  Connection

Waste Sorting Logic

The sorting mechanism is intentionally simple and easy to reproduce.

When paper or cardboard is detected, the servo rotates toward the biodegradable waste compartment. After a short delay, it returns to its neutral position.

When plastic is detected, the servo rotates in the opposite direction, guiding the item into the non-biodegradable collection area.

Battery detection follows a different workflow. Instead of moving the servo, the system activates a buzzer to alert the user that a hazardous item has been identified. This helps prevent improper disposal of batteries, which can release harmful chemicals into the environment.

sorting

Hardware Used

The project can be assembled using commonly available components:

The servo motor serves as the physical sorting mechanism, while the buzzer provides safety notifications for hazardous waste.

components

Training the Object Detection Model

The intelligence behind the project comes from a custom object detection model created using Edge Impulse.

The workflow begins by collecting images of the target waste categories. These images are labeled and used to train a machine learning model capable of recognizing different materials. After training, the optimized model is deployed for real-time inference.

By leveraging machine learning instead of traditional sensors, the system can distinguish visually different objects without requiring separate detection hardware for each material type.

Arduino uno q traning

Software Architecture

The software is divided into two layers.

The Python application handles video capture, object detection, confidence evaluation, and decision-making. It continuously analyzes camera frames and determines when a detection is reliable enough to trigger an action.

The Arduino firmware manages hardware control. It receives commands from the Python application and executes functions such as:

  • Rotating the servo to a specific angle

  • Returning the servo to its default position

  • Activating the buzzer for a defined duration

This separation keeps the microcontroller focused on hardware control while allowing the computer vision workload to run efficiently on the host system.

circuit diagram

Improving Detection Reliability

One challenge in computer vision projects is preventing repeated or accidental activations.

To address this, the system implements:

  • Confidence thresholds for each waste category

  • Consecutive frame validation

  • Cooldown timers between actions

  • Detection debouncing

These techniques ensure that sorting actions occur only when the system is confident about the identified object.

Applications

Although designed as a demonstration project, the same concept can be expanded for larger waste management applications, including:

  • Smart recycling bins

  • Educational STEM projects

  • School and university demonstrations

  • Community recycling programs

  • Small-scale automated waste collection systems

The project also provides a practical introduction to machine learning at the edge, embedded control systems, and real-world computer vision applications.

Final Thoughts

This project demonstrates how embedded AI can be applied to everyday environmental challenges. By combining computer vision, machine learning, and simple electromechanical control, the system can automatically identify and sort common waste materials with minimal user intervention.

Whether you're exploring Edge AI, learning about object detection, or building a sustainability-focused project, this Automatic Waste Segregation System offers an excellent hands-on example of how intelligent automation can improve recycling and resource management.

Objednací č. Mfr ABX00162
ARDUINO UNO Q 2GB RAM 16GB EMMC
Arduino
917,64 Kč
View More Details
Objednací č. Mfr ABX00173
ARDUINO UNO Q 4GB RAM 32GB EMMC
Arduino
1 230,47 Kč
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.