Maker.io main logo

BBC micro:bit Powered Halo-ween Fancy Dress

35

2024-10-24 | By Kitronik Maker

License: See Original Project micro:bit

Courtesy of Kitronik

Guide by Kitronik Maker

Halloween offers the perfect opportunity for some fancy dress fun. In this tutorial, ‎we will show you how this can easily be done using the Kitronik ZIP Halo for the ‎BBC micro:bit.‎

fancydress_1

This will definitely make you the belle of the ball and if you also want venture out to ‎trick or treat, it will help to light your way. ‎

BBC micro:bit Powered Halo-ween Fancy Dress:‎

Parts:‎

Tools:‎

Coding:‎

halo-ween_2

In this tutorial, we are going to show you how to add LEDs to a witches hat, ‎as pictured above, the same techniques can be used to modify other fancy dress ‎items such as capes, as shown above, and at the foot of the tutorial. Let's get ‎making! ‎

Step 1:‎

Once the micro:bit has been connected to the ZIP Halo using the supplied bolts the ‎first task is to connect the extra ZIP LEDs that we will be adding to the hat, to the ‎extension connection point on the ZIP Halo. The extension point is indicated by the ‎text ‘ZIP_EXT’ as shown in the image below. These connections will need ‎connecting to the corresponding connections on the flexible ZIP LED strips.‎

step1_3

To connect the parts together you will need three strands of cable. We have ‎decided to use a male to female servo extension cable to that the hat can be ‎‎‘plugged’ into the ZIP Halo and removed again when not in use. The first task is to ‎cut the extension cable into two halves as shown below.

cut_4

Step 2:‎

Take one-half and strip the insulation from the end of each of the three wires so ‎that it can be soldered the ZIP Halo board.‎ ‎ ‎

step2_5

Step 3:‎

Solder the three wires to the ‘ZIP_EXT’ connection point as shown below. We have ‎chosen to have the wires coming out of the back of the ZIP Halo so that they don’t ‎get in the way of the front LEDs.‎

step3_6

The results will look like this.‎ ‎ ‎

results_7

Step 4:‎

The flexible ZIP strips will need cutting down to fit the size of hat that you are using. ‎This is easy to do as the strips have cut points after each LED as shown below. ‎We will be using one strip on either side of the hat so cut two of the same length.‎

zip_8

Now take the second half of the servo intension cable which we will be soldering to ‎the first section of flexible ZIP strip. It important to make sure the three lines are ‎connected in the correct way. The connections should be made (soldered) as ‎follows:‎

table_9

Also, the flexible strips are directional with data being fed in one end and out the ‎other. This is indicated by the arrows printed on the strip. Make sure you connect ‎to the data in end. The result should look as shown below.

strips_10

Step 5:‎

Now take the second flexible ZIP strip and connect (solder) it to the first piece ‎using three pieces of connecting wire as shown below. Again, take care to ensure ‎the arrows on the strips flow from the ZIP Halo, along the first strip and onto the ‎second strip.‎

step5_11 ‎ ‎

Step 6:‎

Now it is time to carefully position the two LED strip onto the hat. The flexible ZIP ‎strip has an adhesive backing. Peel this away and stick the two strips in the ‎desired positions. The extension connector should be located at the bottom of the ‎hat. When you are happy with the positioning you may wish to sew over the strips ‎‎(not through the PCBs!) in a number of places for extra security.

step6_12

Step 7:‎

Cut a small hole in the hat at the point where the extension cable joins the strips as ‎shown below.‎

step7_13

Then feed the cable through the hole.‎ ‎

feed_14

The resulting hat should look like this.

hat_15

Step 8:‎

Now the hat is complete it is now time to sew the ZIP Halo board in place. Key ‎points that you will want to consider when deciding where to put the ZIP Halo are:‎

  • Does it want to be visible, and do you also want to use the LEDs on the ZIP ‎Halo and micro:bit?‎

  • Where will the batteries be located? We have chosen to use 3xAAA batteries. ‎These are bulkier than a Lithium Polymer battery but much safer to use.‎

Note: The ZIP Halo can also become warm if the LEDs are used to display some ‎colours at maximum brightness. We will use them at a lower brightness to ensure ‎this is not an issue.

With these points in mind, we decided to locate the ZIP Halo at the front of the ‎dress so that the LEDs can shine through the material and be visible. I small pouch ‎was added to hold the batteries.‎

step8_16‎ ‎

Step 9:‎

The code is shown in the embedded MakeCode editor below, if you are having ‎difficulty seeing what's going on, the edit button in the top right will open the code ‎the full editor which should make it easier to see on a small screen. The code that ‎we have created to control the hat and dress is as follows. This uses two variables ‎to control the ZIP LEDs on the hat and dress. The dress is set up to display red all ‎the time (red is a colour that doesn’t generate too much heat) and the hat can swap ‎between display red and rainbow depending on which button on the micro:bit is ‎pressed.‎

step9_17

Microsoft MakeCode | Terms of Use | Privacy | Download

Step 10:‎

Try on and test. Connect the hat to the dress taking care to ensure the power and ‎data connections are connected the correct way around. Insert the batteries into ‎the battery pack and connect to the micro:bit and turn on the ZIP Halo. The dress ‎will now look like this, perfect for some Halloween fun! Below is a collection of ‎photos that we took of the costumes, and I think you'll agree, costume + LEDs = ‎that's more like it!‎

step10_18

Learn more about the author read more » With thanks to Kevin's Daughter Neve for ‎being a good sport and for being patient while the pictures were taken, even when ‎it started raining!‎

©Kitronik Ltd – You may print this page & link to it, but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

Objednací č. Mfr 5625
ZIP HALO FOR THE BBC MICRO:BIT
Kitronik Ltd.
289,70 Kč
View More Details
Objednací č. Mfr 2273
BATTERY HOLDER AAA 3 CELL LEADS
Kitronik Ltd.
35,93 Kč
View More Details
Objednací č. Mfr MICRO:BIT SINGLE
BBC MICRO-BIT V2 SBC BOARD ONLY
Micro:bit
428,90 Kč
View More Details
Objednací č. Mfr 4747
AUTOMATIC SELF-ADJUSTING WIRE ST
Adafruit Industries LLC
245,35 Kč
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.