Maker.io main logo

Arduino LASER Brightness Pulse Width Modulation PWM

2026-03-27 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Arduino ESP32

In this tutorial, we will use a LASER Module connected to Arduino UNO and Visuino to make it change its brightness using Pulse Width Modulation (PWM).

Watch the video!

WARNING: Lasers can be harmful to the eyes, and you should never look directly into the beam!

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

The Circuit

  • Connect the LASER pin [S] to the Arduino digital pin [10]

  • Connect the LASER pin [GND] to the Arduino pin [GND]

The Circuit

Start Visuino, and Select the Arduino UNO board type.

The Visuino: https://www.visuino.eu also needs to be installed. Download the free version or register for a free trial.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino Add Components and Connect

  • Add "Sine Analog Generator" component

  • Set "SineAnalogGenerator1" component frequency to "0.2"

  • Connect "SineAnalogGenerator1" to Arduino Digital pin [10]

In Visuino Add Components and Connect

In Visuino Add Components and Connect photo 2

In Visuino Add Components and Connect photo 3

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino UNO module, the LASER will slowly turn ON and slowly turn OFF.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download and open it in Visuino: https://www.visuino.eu

Downloads

Objednací č. Mfr A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
566,67 Kč
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.