Asi, a 3D Printed Wearable Robot Friend
2021-10-11 | By Odd_Jayy (Jorvon Moss)
License: See Original Project 3D Printing Wearables
Asi, short for Anansi, from the African folklore tale, is a wearable robot that can be worn on your head. I designed Asi to be lightweight and with the ball joint legs strong enough to hold on to your head.
Print the Parts
The first thing is to print the parts. Files can be downloaded here: https://www.thingiverse.com/thing:4996778. Since this is a heavy 3D print project, you will either need a printer.
STLs:
Bottom Ball rack x1
Ball ring X1
Teeth Rack x1
Front Jaw x1
Servo Base x1
Ring x1
Asi Legs x4
Small Asi legs x2
Logo Head x1
Eyes x1
Screws:
6x5-Bolt x6
Nuts x6
Electronics:
Adafruit Trinket x1
Servo x1
LEDs x4
Battery x1 (I prefer Adafruit lithium batteries)
Assembly
After you print your parts, I recommend gluing the Bottom sections together as shown.
As I have stated before, this is a heavy 3D print project, so I recommend printing these parts and the legs first because it's the fastest way. Once you print the legs, attach them with the screw and bolt. If everything was done correctly, you should have these parts on your desk.
The Electronics
I used the same circuit and code for the Asi bots that was used in a Zelda build on Adafruit, so PLEASE take a look. (https://learn.adafruit.com/guardian-robot-zelda-botw/circuit-diagram)
Of course, I recommend putting the circuit together first, but make sure you print the eye sockets and glue the LEDs inside them before attaching the full circuit. You will want to make sure the wires can reach.
Fit the circuit inside the open area of the Ball ring.
Next, get the servo and the printed servo base. Stick the servo into the base and attach it to the ball ring. I recommend using hot glue. There is a cut in the servo base where the wires can slide through.
Make sure you test the circuit to make sure the servo works, and the LEDs light up.
Attach a servo horn to the top of the Asi Head
Attach the servo from the base to the head. If you have trouble aligning the holes, take the servo out of the holder, attach it to the head, then slide it back into the servo holder.
It may look a little off, but that's fine. The final piece, the “Ring”, goes over the head, hiding the uneven part.
Then you’re done. I hope this was easy to follow along with, but you can check out the video of the Asi Spider bot for more info.