Let’s Abuse a Battery! - Experiment 2
For those of you who missed my first blog, “Taste the Power! – Experiment 1”, I recently got the second edition of “Make: Electronics” by Charles Platt and decided to try all of the experiments presented in the book. This is my documentation of how the second experiment turned out.

Before we begin, for those who might be thinking of ignoring Mr. Platt’s advice and want to see what happens when you short a lithium battery, just watch this AWESOME video instead:
How to blow a fuse

I used two different 1.5 V AA brand new batteries, but unfortunately, I was unable to blow the 3 A fuse (I even tried with a 9 V battery).



Luckily, I had a 1 A fuse at home, which did burn, but only by applying the wires from the battery holder to it directly.
The reason I wasn’t able to blow the fuse with the test leads could be that some cheap test leads don’t allow enough current to flow through them.
The book has so far introduced us to batteries and fuses. To learn more about these components you can check out chapters 2 and 4 of Charles Platt’s “Encyclopedia of Electronic Components Volume 1”.
If you would like to recreate this experiment yourself, you can get everything you need for this experiment from DigiKey!
- 1.5 V AA Batteries
- Battery carrier
- 3 A Automotive Fuse
- Safety Glasses
- Test leads with alligator clips at each end
EXTRA
If you would to explore this topic some more, check out the links below.
Why do Lithium-ion batteries explode
https://www.howtogeek.com/338762/why-do-lithium-ion-batteries-explode/
Types of fuses
https://www.electronicshub.org/fuses-types-fuses/
How batteries work
https://www.youtube.com/watch?v=9OVtk6G2TnQ
Alessandro Volta – The Battery
https://www.youtube.com/watch?v=Is8wAeoTqHQ
Solid state electronics
https://en.wikipedia.org/wiki/Solid-state_electronics
Surface mount technology
https://en.wikipedia.org/wiki/Surface-mount_technology
AC Power plugs and sockets
https://en.wikipedia.org/wiki/AC_power_plugs_and_sockets
The Voltaic pile
https://libraries.mit.edu/collections/vail-collection/topics/electricity/the-voltaic-pile/
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum